Other Parts Discussed in Thread: TPS3808
Dear Sir, please answer
I need to add a hysteresis in TPS3803-01. Power supply is 3.6 – 2.4 V. I need to set a threshold voltage 2.7 V and to add a hysteresis.
I use TPS3808 application, as I assume, that the logic of operation of these microcircuits is the same. (in my case V1 = V2, please, see figure 1, page 2 of TPS3808 application). On the page 4 assigned the following values: V1+ = 2V, V1- = 1.8V.
Please see Figure 2 of TPS3808 application, page 2:
R1 connected to V1+ voltage (it's 2V in this example).
If I understand right, RESET output must be HIGH at V1+ (it's 2 V ), but according to Figure 2 - this is a LOW level. And in figure 3 (page 3), in my opinion, it should be the other way around. I understand that, if the input voltage is only applied and it starts to grow, then RESET output is LOW, until the supply reaches 2 V, but Figure 2 shows the voltage V1+ =2V, i.e. voltage at which the RESET output must be HIGH. Please, explain.
TIA
Sincerely,
Vladimir Naumenkov