This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hey Guy,
Question 1: The min and max allowable capacitance for your system would need to be determined using a small signal measurement conducted on the EVM.
For minimum output capacitance the loop crossover frequency must be less than one-half of the switching frequency (300 kHz), and the phase margin at the loop crossover must be greater than 50 degrees.
For maximum output capacitance, adopt an extremely high output capacitance and lower or raise depending on if the phase margin loop crossover is greater than 50 degrees. (> 50 degrees means the system will be stable.)
I would say to design your system based on your ripple and transient requirements then adjust for stability.
See section 7.3.3 of the datasheet for more information.
Question 2: You won't need to feed a voltage at the output of the inductor using a separate trace (red line) Just connect the VO, and FB node to the point that you would like to regulate at. If you are regulating at the load, then all you will need is the blue trace and the yellow trace seen in your diagram.
Thanks,
Caleb
Hi Caleb,
Thanks for getting back to me so quickly.
I understand that the minimum requirements need to meet the crossover/phase margin requirements. How do I calculate the crossover frequency and phase margin? I have tried using the WEBBENCH, but it does not run frequency domain analysis. Thanks.
Hey Guy,
I'll be closing this thread since we're communicating through email now.
Thanks,
Caleb