If we are using 4S battery, the output voltage of NVDC is about 17.8V and system w/ 100W(20V@5A) adapter.
Also the system input voltage is dropped to around 18V when the total system power is increased close to 100W and the large current happens suddenly.
In this case, since the output voltage of NDVC is nearly equal to the system input voltage, NVDC will work in the buck-boost mode then the inductor current is increased.
Is there no problem on the inductor thermal rise/saturation?
Would you help to calculate this worse case inductor current and △IL on this case?