I am using the BQ24095 to charge a single cell battery.
However there is a case if the battery goes below 3V the protection circuit of the battery kicks in and shuts down the battery, effectively making it an "open circuit". The issue with this is that when I plug in the USB cable to charge the battery the output voltage of the BQ24095 only gets to 200mV, so the battery is never charged.
I suspect that the system circuit during power up may be drawing an excess current spike that the device thinks is a short circuit. Unfortunately, I am not able to confirm this as the PCB layout and components don't allow me to test for this.
I have confimed by removing the battery that the BQ24095 IC is not able to power my unit by itself, even though it draws less than the 1000mA that the charger IC is set to via the ISET resistor value. I have also changed the PRE-TERM resistor to a 10k, meaning that the pre charge current will be 1000mA as well.
I am not able to find any information on how the BQ24095 determines if there is a short circuit or not. There is a mention of doing a 100mA short circuit test at power up, but no specifics.
Is there any information that you are able to provide on this please?
Many thanks,
Sean