Other Parts Discussed in Thread: TPS61202
The BQ24095 has a number of short circuit protection features build in. In the datasheet there is a mention that the IC does a 100mA short circuit detection. What are the parameters for this test to return a short circuit result ending in the chip being shut down and needing to be power cycled in order to be unlatched?
The datasheet gives no indication of the conditions needed to warrant a short circuit.
Any supporting material of documentation would be apprecitated if possilbe.
Many thanks,
Sean