Other Parts Discussed in Thread: TPS61098
hi:
TPS610986, input 1.5V, output 3.3V, VSUB is followed by a load of 3-5mA,
MODE is low, some VSUBs have charging and discharging waveforms, and some have high levels.
How to understand this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
I think it may not an expected behavior of TPS61098.
There are several things I want to check,
what is connected with MODE pin? Is it a MCU IO pin or some other things?
Is there any load on VMAIN? Is VMAIN a stable 3.3V?
Regards,
Nathan
hi:
1. what is connected with MODE pin? Is it a MCU IO pin or some other things?
MCU IO.
2.Is there any load on VMAIN?
yes
3.Is VMAIN a stable 3.3V?
yes
Hi Kevin,
So what the load current from VMAIN?
And more, in condition 2 and condition 3, MODE are both logic low level, but the VSUB conditions are different, what the setup differences between this two conditions?
Nathan
hi Nathan:
1. So what the load current from VMAIN?
normal: 50 mA, standby:60 uA.
2.And more, in condition 2 and condition 3, MODE are both logic low level, but the VSUB conditions are different,
what the setup differences between this two conditions?
The difference is that customers want to know why?
Hi kevin,
Ok, I knew, sorry that I got something wrong about your question before.
So does this mean that customer tried several chips and some chips get high level but some chips don't get, or that customer only tried one chip and sometimes get high level but don't get high level other times?
some VSUBs have charging and discharging waveforms, and some have high levels.
Regards,
Nathan
hi Nathan:
total 6000 PCS,MODE PIN LOW, 57% VSUB PIN LOW or charging and discharging waveforms, 43% VSUB PIN HIGH.
Hi Kevin,
Does customer check that the mode pin voltage < 0.4V? Maybe the logic low voltage level not exactly equal to 0 due to noise.
Nathan
Hello Kevin,
As we did not hear back from you, I expect the issue is solved and I will close this thread. If you have further questions, please post below or start a new thread.
Best regards,
Brigitte