Other Parts Discussed in Thread: TPS549D22
Hi Peter,
I am measuring excessive ripple on all my 3 rails. (0.9V quad, 1.0V quad, and 1.2V single), mainly because the consumption is currently too low.
Typical rail configuration: 0.9V, consumption: designed for 160A but currently drawing 2A, quad phase , FSW=650KHz, L=150nH, MPN: VLBU1007090T-R15L ( https://product.tdk.com/en/search/inductor/inductor/smd/info?part_no=VLBU1007090T-R15L ), Cout= 42,053uF (10 x 3300uF Alum-poly, 2 x 820uF Alum-poly, 2 x 680uF Alum_poly, 6 x 470uF alum-polymer, 28 x 100uF ceramic, 8 x 47uF Ceramic, 10 x 4.7uF Ceramic, 10 x 1uF Ceramic, and some nF range caps).
The current consumption as mentioned above is super low right now, the regulator is at FPWM mode, is it the only mode the part supports? do I have to change the compensation (we are at 14) to reduce the ripple within range? Reduce Fsw?
My max load current is estimated to be around 80A-100A.
Thanks,
Bahram
TPS546D24A_ExcelCalculator_SchematicLayoutChecklist_P0V9_06-07-2022 .xlsx