Hi,
I am using BQ25895MRTWR in our project. In that, we are facing an issue.
HARDWARE DETAILS
IC: BQ25895MRTWR
BATTERY: 3.7V/5000mAh Rechargeable Lithium Polymer Battery Cell.
Link:https://www.innovoya.com/product-page/955465-5000mah-rechargeable-lithium-polymer-battery-cells-1
VBUS connected to the type-c connector(5V)
schematics attached.
ISSUE
While we connect a battery that is less than 2V. It will charge up to 2.99V and stops charging.
ie, trickle charging and recharging happened. But no change afterward.
I2C configuration is as default. Since we are not configured anything through I2C.
Could you please help us to resolve the issue?
Will the IC, charge the battery in the default configuration?