This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31506: No voltage output from VOUT port

Part Number: LMZ31506


The board was working fine, but at some point the LMZ31506RUQR's VOUT output (+3.3V) went to 0V.


・When I measured the resistance value between VOUT and GND after it became 0V, it was 1.9Ω.
・The resistance value between VOUT and GND of the board in normal operation was 311Ω.
・+3.3V is input to INH/UVLO.
・+12V is input to VIN.
・When I probed the PH port, it was fixed at 0V.
・The overcurrent protection circuit is not operating, and there is no periodic voltage fluctuation of VOUT.

What could be the cause of the problem with the LMZ31506RUQR?

Please let me know if there is anything I should check with LMZ31506RUQR.

I'll attach a schematic excerpt.