HI There,
Quick question. If someone is using the LM74502-Q1 as a surge stopper in Section 10.3 (Figure 10-11) of the datasheet, and the VS is clamped at 60V through the Dz and R1, is there still a requirement to have a negative clamping TVS (along with blocking diode) on Vbatt input supply as shown in Figure 10-2?
This is to clamp transients that go below -65V...
Thanks for the sanity check...