Other Parts Discussed in Thread: TPS54360
Hi Team,
My setup,
Vin->TPS54360B->Battery Charger | Load | LDO
Functionality:
Q8 is OFF when Vin is ON and TPS5360B is giving an output.
Q8 is ON when there is no output form TPS54360B.
My issue:
Question 1:
When Q8 is ON, the battery voltage will reach PIN 8 SW of TPS54360B and also the PIN 1&2 of battery charger IC,
Is there is any possibility that the battery voltage that is of Li-ion battery of 4.2V max at PIN SW of TPS54360
might damage the TPS54360B IC and affect its ON operation in any way?
Question 2:
Do we need to protect the TPS54360B PIN 8 SW from any voltage source connection?
Kindly clarify,
Many thanks
Swaroop