We are using LP5907MFX-1.8/NOPB in our design. Please review our schematic and give us your valuable feedback as soon as possible
Kindly find the attached schematic pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are using LP5907MFX-1.8/NOPB in our design. Please review our schematic and give us your valuable feedback as soon as possible
Kindly find the attached schematic pdf
Hi Siddhi,
I looked at the schematics and here is some of my feedback:
1) What is the load for LP5907? 3) It is recommended to use a capacitance of 0.7uF to 3uF with a minimum and maximum ESR of 1mOhm to 500mOhm for a load range of 400uA to 2mA. If the load is higher, then the minimum and maximum recommended capacitance is 1uF to 10uF.
2) NC can be tied to GND for thermal improvement, if needed.
Note that I am using capacitance and not capacitor, although the capacitors used seem to be ok, this is important to keep a note on.
Other than that, the schematic looks good.
Best,
Edgar Acosta