Is there short test data for bq25300 on below condition?
・Adjacent pin to pin short
・SW to GND short
・BAT to GND short
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Satoshi,
I do not have a customer friendly report available. There are protections to prevent damage from SW and BAT being shorted to GND. The only pin to pin shorts that result in IC damage are BTST to GND (thermal pad) and PMID to BTST.
Regards,
Jeff
Hi Jeff
Thank you for reply,
Please let me know about additional question and request below;
・Is there any test waveform for short circuit protection the other than figure 10-6?
Customer want to reference the these test data as much as possible.
・If in the case of BTST pin ~ PMID pin short, or BTST pin ~ GND short, is this possibility to cause battery overload?
Or, is it occur only IC damage?
Best regards,
Satoshi