Hi,
I intend to connect only three cells to the BQ76952EVM evaluation board.
I see that minimum of three cells are to be connected to the board.
So, if I have three cells- Cell A, B and C. My connection would be as follows -
Cell A (-ve) to BAT- (J4.6)
Cell A (+ve) / Cell B (-ve) to CELL1 (J4.5)
Cell B (+ve) / Cell C (-ve) to CELL2 (J4.4)
Cell C (+ve) to CELL16 (J1.1)
1. I have removed all the shunts from cell simulator pins (J14 and J23) since I am using the actual battery cells. Please let me know if I am right.
2. Should I also be shorting the pins (J1.1,2,3,4,5) to (J3.1,2,3,4,5) and (J4.1,2,3,4) or leave them open?