We are using the TPS62840DLC on a design and because it meets the requirements and the space constraints. There may be are reason we want to up the output voltage slightly above 3.3V.
Is there undocumented resistors that would allow a higher voltage than 3.3V? Switching to the TPS62842DGR is not really and option.
Is there going to be TPS62842DLC? so that it can be in the same package size?