Dear Specialists,
My customer is considering changing ULN2803A to ULN2803C and has questions.
I would be grateful if you could advise.
---
(1) Input voltage (Vi), junction temperature (Tj) recommended operating conditions for ULN2803CDWR are the same as the discontinued ULN2803ADWR?"
According to the datasheet of ULN2803C, Junction temperature range is not described.
(2) the descriptions are different, Vcc for ULN2803A and Vce for ULN2803C, but are they showing the same collector-emitter voltage?
Recommended Operation Conditions for ULN2803A, Vcc is listed.
Recommended Operation Conditions for ULN2803C, VCE is listed.
(3) When GND or power supply (5V or 12V or 24V) is connected to the NC pin, is there a problem?"
*We are considering whether it can be mounted without changing the board pad, and we would like to check whether there is any impact even if there is a GND or power via directly under the NC pin.
---
I appreciate your great help in advance.
Best regards,
Shinichi