hi,
Does TUSB1046A-DCI need 2Mohm for SBU1/2?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you for your reply.
Please tell me one more thing.
I've checked the TUSB1046A-DCI and USB specs and couldn't find any reason why PD resistor is needed.
Where in the TUSB1046A-DCI and USB specifications did you find that you needed a PD resistor? can you tell me that.
(I couldn't find the reason I needed 2Mohm.
TUSB1046 spec just write "SBU1. This pin should be DC coupled to the SBU1 pin on the Type-C receptacle. A 2-M ohm resistor
to GND is also recommended."
And also, input AUXP/N have 100kohm Pu/Pd that's why I don't know why need 2M ohm.
Perhaps it is necessary because the TUSB1046 was not powered and there was an Aux connection from the TypeC connector?)