This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51420: Low Freq Ripple of LMR51420XDDCR

Expert 1215 points
Part Number: LMR51420
Other Parts Discussed in Thread: LMZM23600EVM, LMZM23600

Hello,

I am using LMR51420XDDCR to step down voltage from 21V to 3.3V using 8.2uH inductor and 88uF MLCC at output.

I have light load of 60mA.

With that condition I am getting 20mV low frequency output voltage ripple like in the picture:

To reduce that I can add second LC filter or LDO at output... but looking on the LMZM23600EVM (21Vin,3.3Vout, FPWM) board there is only 69uF at output and there is no low frequency ripple:

So based on LMZM23600EVM dev board there must be the way to reduce Low Frequency Ripple without using LDO or 2nd filter. Why on LMZM2600 this low freq ripple is not visible?

Is there a way for me to have with LMR51420XDDCR similar low freq ripple as on LMZM23600EVM without adding LDO or 2nd filter?

Adam