This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27421-G1: differences between BQ27421 and BQ27427

Part Number: BQ27421-G1
Other Parts Discussed in Thread: BQ24210, BQ27220, BQ27427, GPCCHEM

I have a solar-powered project that is using a BQ24210 charger, we were considering using the BQ27220 fuel gauge,

but after considering device age, availability and integrated sense resistor we would like to consider the BQ27421. Is this 

an acceptable device for use with the BQ24210? Additionally, how do the BQ27421 and the BQ27427 differ and are these

devices interchangeable? It looks like they are pin compatible.

Thanks