I have the following question regarding the LM51501 DC/DC Controller:
On page 11 of the datasheet, the following is stated:
“The wide input range of the
device covers automotive load dump transient.”
From ISO 16750-2:2010(E), a load dump may reach from 151V / 1 ohm to 202V / 8 ohm in a 24 V system or 79V / .5 ohm to 101 / 4 ohm in a 12V system.
Can the LM51501 survive these levels?