This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90124: UCD90124

Part Number: UCD90124
Other Parts Discussed in Thread: UCD90120, , UCD90120A,

Hello Experts, UCD90124 is pin, footprint compatible with UCD90120. Can we program the NVRAM of UCD90124 multiple times? Which version of Fusion designer supports UCD90124?

Even if this being an old part, this part is available in market.

thanks, Abhijit

  • HI

    UCD90124 is P2P to UCD90120 but with different feature set. you can not mix these two devices.

    The NVRAM has 20K min cycles.

    It is the same UCD90120 which was shared in the separated post.

    Regards

    Yihe

  • Hi Yihe, I am an ex TIer. ID: a0393757. I have ordered UCD90124 from mouser to replace the UCD90120 on my boards. Mouser is an authorised distributor correct?

    How to know that a part is a valid TI part?

    Is it possible to have a short call today?

    i am in Bangalore, India.

     Thanks, Abhijit 

  • Hi

    I would recommend UCD90124A or UCD90120A since they have more features and support.

    The UCD90120 and UCD90124 have very limited support unfortunately.

    As long as the parts were purchased from TI's legal distribution channel, it shall be fine.

    Regards

    Yihe