What is normal position of BOOT Switch in the EVM?
What to do if you have to remove the BOOT switch?
Is there a provision to operate the EVM without BOOT switch?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is normal position of BOOT Switch in the EVM?
What to do if you have to remove the BOOT switch?
Is there a provision to operate the EVM without BOOT switch?
Hello,
TS1 is needed as an input to boot the part. A 1- to 100-kΩ pulldown may be suitable.
What is normal position of BOOT Switch in the EVM?

What to do if you have to remove the BOOT switch?
The BOOT switch is needed for the part to turn ON.
Please refer to this FAQ user guide and this app note for alternative boot switches circuitry.
Regards,
Jose Couso