This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5860: Current rating of SW pin

Part Number: LP5860

Hi team,

My customer has been designing with LP5860.

Do we have the current rating of SW pin? Since there is only curent rating of CS pin on the datasheet.

Best regards,

Shunsuke Yamamoto

  • Hi Yamamoto,

    The current sink can generate current up to 50mA, and each SW connect to 18 CS, so SW is able to handle up to 18*50mA current.

    I don't have the exact number of SW pin current rating, but it is enough to handle the device for proper operation.

     

    Best Regards,

    Ives