Hi
My customer's application is for 24V car, the surge test requirement is +150V and -450V pulse.
Can LM74501-Q1 adding some external component pass +150V and -450V pulse test ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer's application is for 24V car, the surge test requirement is +150V and -450V pulse.
Can LM74501-Q1 adding some external component pass +150V and -450V pulse test ?
Hi PYTsai,
Can you share more details about the pulses - time duration of peak voltage, impedance in between the test circuit and the device, etc..
If we can can clamp the voltages seen at the input of LM74501-Q1 using input TVS or input capacitance or the VDS clamp circuit or a combination of all of these to less than the device Abs Max rating then there should be no issue.
Please note that LM74501-Q1 can meet automotive ISO7637-2 pulse 1 transient without additional TVS diode