Hi,
As title, I would like to know TPS7A39 suitable for this application?
1. Vin 21.7~22.3V to Vout 14.5~15.5V
2. Vin -7.3~-6.7V to Vout -13.5~-12.5V
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
edit to clarify thermal values & negative LDO capability
Hi Jeff,
TPS7A39 is suitable for this application. Voltages are within range and device thermals can support this.
Power Dissipation:
Junction Temperature:
1. PD = (21.7 - 14.5) * 0.15 = 1.08W or PD = (22.3 - 15.5) * 0.15 = 1.02W
125°C = TA + 44.4 * 1.08 or 125°C = TA + 44.4 * 1.02
This is not possible unless the voltage drop is decreased so that the device temperature is within operating range.
2. A negative LDO cannot regulate from a greater negative value to a lesser negative value, ie -7.3 to -13.5. The inverse, however is possible and the LDO could regulate from -13.5 to -7.3.
I hope this is helpful,
Erin