I have query regarding alternative to 56PR3362.
Please suggest an alternative or guide from which suppliers I can this part.
I am not able to find an alternative having insulation as well as low leakage inductance.
Also, as per other threads, it is found that its customized as per original part no. AF4779_032807
I also want to know why in customized part input inductance is 1.3 mH then actual part number which is 0.9 mH.