Other Parts Discussed in Thread: UCD3138,
Hello everyone,
I am trying to build a PSFB using the UCD3138A64. However, quite surprisngly I am not able to find any example codes for the same. Unlike C2000 controllers, where after explaining each section, TI gives nicely commented example code, I can't find anything similar on the UCD3138 side. Yes there are reference desings avialble but they do little to help a beginner who has just started the UCCD3138 coontroller. A full fledged project is much more difficult to keep track of and understand especially when TI says that a detailed manual is provided, which, without a doubt, is missing. The user just has to depend on the few shortly commented lines of code.
I would request TI represenatives to create a a proper examples for each part of the reference manual( similar to the C2000 devices). Much of the potential of the device is lost without example codes.
For now, I would be grateful if someone could send me a basic example code for the phase shifted full bridge. I just want the basic configuration in the open loop mode, to which later I can change the phase shifts later through the Hyperknob in the memory debugger.