Hi,
We encounter bad balancing times on our BMS. All balancing parameters are met, but still the CB bit is often not active. It seems like the balancing algorithm only balances away a single high cell, but does not account for a single low cell.
Typical for this problem is:
1. After a discharging current, the CB bit is for 60s continue on.
2. After 60s of charging, the bit will toggle some times.
With that knowledge, I once balanced a pack with a battery tester by charging 1m, then discharge for 1s and repeat. Without problems.
But I have never seen a customer doing that.
I have included some logs showing the problem. I am currently trying the R3 firmware, wich is no different. Also we can't get the feature of R3 to work.
Above all the settings for balancing.
Mon Jan 23 14:01:26 CET 2023 Device Version Info = 1e9b_3_00 BQZ Device Name = bq78350R3 BQZ Firmware Version = V3_00_BLD31 Design Capacity = 1050 Design Voltage = 3200 Specification Info = 0x1031 Manufacturer Date = 2022-12-22 Serial Number = 0x0100 Manufacturer Name = ES024105-04 Device Name = 22110100 Device Chemistry = F174 Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,RunTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,PendingEdv,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFStatAB,CellVolt1,CellVolt2,CellVolt3,CellVolt4,CellVolt5,CellVolt6,CellVolt7,CellVolt8,CellVolt9,CellVolt10,CellVolt11,CellVolt12,CellVolt13,CellVolt14,CellVolt15,ExtAvgCellVolt,TS1 Temp,TS2 Temp,TS3 Temp,CellTemp,FetTemp,CB_REST_Enable,CB_REST_Enable,LogRowTime(ms),LogStatus 1,2023-01-23 14:01:30,4.001,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28769,67,71,100,100,100,1050,1050,65535,65535,0,44,29200,0x40A0,0,0,100,0x0107,0x8000,0x10,0xC8,0x1A,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3439,3611,3628,3667,3661,3494,3648,3622,0,0,0,0,0,0,0,3599,27.4,32.0,-273.2,32.0,27.4,0x00,0x00,974,SUCCESS 2,2023-01-23 14:01:34,8.002,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28772,63,70,100,100,100,1050,1050,65535,65535,0,44,29200,0x40A0,0,0,100,0x0107,0x8000,0x10,0xC8,0x1A,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3438,3611,3629,3668,3661,3493,3648,3622,0,0,0,0,0,0,0,3598,27.4,32.0,-273.2,32.0,27.4,0x00,0x00,976,SUCCESS 3,2023-01-23 14:01:38,12.002,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28777,67,69,100,100,100,1050,1050,65535,65535,0,44,29200,0x40A0,0,0,100,0x0107,0x8000,0x10,0xC8,0x1A,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3438,3613,3630,3669,3662,3493,3650,3623,0,0,0,0,0,0,0,3599,27.3,32.0,-273.2,32.0,27.3,0x00,0x00,991,SUCCESS 4,2023-01-23 14:01:42,16.003,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28779,63,68,100,100,100,1050,1050,65535,65535,0,44,29200,0x40A0,0,0,100,0x0107,0x8000,0x10,0xC8,0x1A,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3437,3613,3631,3670,3663,3492,3650,3623,0,0,0,0,0,0,0,3599,27.3,32.0,-273.2,32.0,27.3,0x00,0x00,976,SUCCESS 5,2023-01-23 14:01:46,20.003,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28796,64,67,100,100,100,1050,1050,65535,65535,0,44,29200,0x40A0,0,0,100,0x0107,0x9000,0x10,0xC8,0x1A,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3437,3614,3633,3671,3681,3492,3651,3624,0,0,0,0,0,0,0,3599,27.3,32.0,-273.2,32.0,27.3,0x00,0x00,975,SUCCESS 6,2023-01-23 14:01:50,24.004,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28803,62,66,100,100,100,1050,1050,65535,65535,0,44,29200,0x40A0,0,0,100,0x0107,0x9000,0x10,0xC8,0x1A,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3436,3615,3633,3672,3682,3492,3652,3624,0,0,0,0,0,0,0,3599,27.2,32.0,-273.2,32.0,27.2,0x00,0x00,990,SUCCESS 7,2023-01-23 14:01:54,28.005,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28778,30,65,100,100,100,1050,1050,65535,65535,0,44,29200,0x40A0,0,0,100,0x0107,0x9000,0x10,0xC8,0x1A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3431,3610,3628,3666,3664,3487,3647,3619,0,0,0,0,0,0,0,3591,27.3,32.0,-273.2,32.0,27.3,0x00,0x00,968,SUCCESS 8,2023-01-23 14:01:58,32.005,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28644,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3425,3593,3610,3648,3642,3478,3630,3603,0,0,0,0,0,0,0,3576,27.3,32.0,-273.2,32.0,27.3,0x00,0x00,973,SUCCESS 9,2023-01-23 14:02:02,36.005,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28548,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3421,3581,3596,3633,3627,3470,3617,3590,0,0,0,0,0,0,0,3566,27.2,32.0,-273.2,32.0,27.2,0x00,0x00,973,SUCCESS 10,2023-01-23 14:02:06,40.006,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28466,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3416,3571,3584,3619,3614,3468,3605,3579,0,0,0,0,0,0,0,3556,27.2,32.0,-273.2,32.0,27.2,0x00,0x00,971,SUCCESS 11,2023-01-23 14:02:10,44.006,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28395,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3413,3561,3574,3608,3604,3461,3595,3569,0,0,0,0,0,0,0,3546,27.3,32.0,-273.2,32.0,27.3,0x00,0x00,974,SUCCESS 12,2023-01-23 14:02:14,48.006,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28330,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3409,3553,3564,3598,3594,3455,3587,3560,0,0,0,0,0,0,0,3537,27.3,32.0,-273.2,32.0,27.3,0x00,0x00,972,SUCCESS 13,2023-01-23 14:02:18,52.006,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28270,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3406,3545,3556,3589,3585,3451,3579,3552,0,0,0,0,0,0,0,3532,27.2,32.0,-273.2,32.0,27.2,0x00,0x00,970,SUCCESS 14,2023-01-23 14:02:22,56.007,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28217,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3403,3538,3547,3580,3577,3447,3572,3545,0,0,0,0,0,0,0,3527,27.2,32.0,-273.2,32.0,27.2,0x00,0x00,970,SUCCESS 15,2023-01-23 14:02:26,60.007,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28166,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3400,3531,3540,3572,3570,3443,3564,3539,0,0,0,0,0,0,0,3518,27.2,32.0,-273.2,32.0,27.2,0x00,0x00,971,SUCCESS 16,2023-01-23 14:02:30,64.007,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28121,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3399,3525,3533,3565,3562,3440,3557,3532,0,0,0,0,0,0,0,3513,27.2,32.0,-273.2,32.0,27.2,0x00,0x00,970,SUCCESS 17,2023-01-23 14:02:34,68.008,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28080,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3396,3519,3528,3559,3555,3436,3554,3526,0,0,0,0,0,0,0,3508,27.2,32.0,-273.2,32.0,27.2,0x00,0x00,970,SUCCESS 18,2023-01-23 14:02:38,72.009,0x0701,20,10,0x6001,0,65535,65535,1,32.0,28037,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3394,3513,3521,3552,3551,3433,3547,3520,0,0,0,0,0,0,0,3503,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,968,SUCCESS 19,2023-01-23 14:02:42,76.009,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27999,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3392,3511,3516,3546,3544,3431,3541,3515,0,0,0,0,0,0,0,3499,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,968,SUCCESS 20,2023-01-23 14:02:46,80.010,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27966,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3391,3505,3511,3541,3538,3428,3536,3511,0,0,0,0,0,0,0,3494,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,969,SUCCESS 21,2023-01-23 14:02:50,84.010,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27928,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3389,3500,3505,3535,3532,3425,3531,3506,0,0,0,0,0,0,0,3489,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,968,SUCCESS 22,2023-01-23 14:02:54,88.010,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27899,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3387,3496,3502,3530,3527,3422,3528,3501,0,0,0,0,0,0,0,3484,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,980,SUCCESS 23,2023-01-23 14:02:58,92.010,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27870,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3386,3492,3497,3525,3524,3420,3523,3497,0,0,0,0,0,0,0,3479,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,967,SUCCESS 24,2023-01-23 14:03:02,96.011,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27838,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3385,3486,3492,3520,3519,3418,3519,3493,0,0,0,0,0,0,0,3479,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,969,SUCCESS 25,2023-01-23 14:03:06,100.012,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27812,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3383,3485,3489,3517,3515,3416,3515,3489,0,0,0,0,0,0,0,3475,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,965,SUCCESS 26,2023-01-23 14:03:10,104.012,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27785,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3382,3481,3484,3513,3510,3414,3511,3486,0,0,0,0,0,0,0,3470,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,965,SUCCESS 27,2023-01-23 14:03:14,108.013,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27758,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3380,3478,3481,3509,3506,3412,3508,3483,0,0,0,0,0,0,0,3470,27.1,32.0,-273.2,32.0,27.1,0x00,0x00,967,SUCCESS 28,2023-01-23 14:03:18,112.013,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27737,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3379,3474,3476,3505,3503,3410,3504,3479,0,0,0,0,0,0,0,3465,27.0,32.0,-273.2,32.0,27.0,0x00,0x00,964,SUCCESS 29,2023-01-23 14:03:22,116.013,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27714,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3378,3472,3475,3501,3500,3409,3501,3476,0,0,0,0,0,0,0,3460,27.0,32.0,-273.2,32.0,27.0,0x00,0x00,979,SUCCESS 30,2023-01-23 14:03:26,120.014,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27691,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3377,3468,3471,3497,3496,3408,3498,3473,0,0,0,0,0,0,0,3460,27.0,32.0,-273.2,32.0,27.0,0x00,0x00,965,SUCCESS 31,2023-01-23 14:03:30,124.014,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27669,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3376,3466,3468,3493,3492,3406,3495,3470,0,0,0,0,0,0,0,3455,27.0,32.0,-273.2,32.0,27.0,0x00,0x00,964,SUCCESS 32,2023-01-23 14:03:34,128.014,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27649,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3374,3463,3465,3491,3489,3404,3493,3468,0,0,0,0,0,0,0,3455,26.9,32.0,-273.2,32.0,26.9,0x00,0x00,963,SUCCESS 33,2023-01-23 14:03:38,132.014,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27630,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3461,3462,3487,3486,3403,3490,3468,0,0,0,0,0,0,0,3451,26.9,32.0,-273.2,32.0,26.9,0x00,0x00,964,SUCCESS 34,2023-01-23 14:03:42,136.016,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27614,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3458,3459,3484,3482,3402,3487,3468,0,0,0,0,0,0,0,3451,26.9,32.0,-273.2,32.0,26.9,0x00,0x00,978,SUCCESS 35,2023-01-23 14:03:46,140.016,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27595,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3456,3457,3481,3482,3400,3483,3463,0,0,0,0,0,0,0,3446,26.9,32.0,-273.2,32.0,26.9,0x00,0x00,974,SUCCESS 36,2023-01-23 14:03:50,144.016,0x0701,20,10,0x6001,0,65535,65535,1,32.0,27584,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3454,3454,3479,3482,3400,3483,3460,0,0,0,0,0,0,0,3446,26.9,32.0,-273.2,32.0,26.9,0x00,0x00,977,SUCCESS 37,2023-01-23 14:03:54,148.017,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27571,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3451,3452,3476,3478,3398,3483,3457,0,0,0,0,0,0,0,3442,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,978,SUCCESS 38,2023-01-23 14:03:58,152.017,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27555,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3449,3449,3474,3475,3397,3482,3455,0,0,0,0,0,0,0,3441,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,976,SUCCESS 39,2023-01-23 14:04:02,156.017,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27538,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3446,3447,3471,3472,3396,3478,3453,0,0,0,0,0,0,0,3441,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,975,SUCCESS 40,2023-01-23 14:04:06,160.017,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27522,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3444,3444,3469,3469,3395,3475,3450,0,0,0,0,0,0,0,3436,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,977,SUCCESS 41,2023-01-23 14:04:10,164.018,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27508,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3372,3442,3442,3466,3467,3394,3473,3448,0,0,0,0,0,0,0,3436,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,975,SUCCESS 42,2023-01-23 14:04:14,168.018,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27494,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3371,3442,3440,3464,3464,3393,3471,3446,0,0,0,0,0,0,0,3436,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,976,SUCCESS 43,2023-01-23 14:04:18,172.019,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27481,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3370,3442,3437,3462,3463,3392,3469,3445,0,0,0,0,0,0,0,3432,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,975,SUCCESS 44,2023-01-23 14:04:22,176.020,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27469,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3369,3442,3435,3459,3461,3390,3468,3443,0,0,0,0,0,0,0,3432,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,974,SUCCESS 45,2023-01-23 14:04:26,180.020,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27457,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3368,3441,3433,3457,3458,3390,3466,3441,0,0,0,0,0,0,0,3432,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,973,SUCCESS 46,2023-01-23 14:04:30,184.020,0x0701,20,10,0x6001,0,65535,65535,1,31.9,27441,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3368,3438,3431,3455,3456,3389,3464,3439,0,0,0,0,0,0,0,3427,26.9,31.9,-273.2,31.9,26.9,0x00,0x00,971,SUCCESS 47,2023-01-23 14:04:34,188.021,0x0701,20,10,0x6001,0,65535,65535,1,31.8,27433,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3368,3436,3431,3453,3454,3389,3462,3438,0,0,0,0,0,0,0,3427,26.9,31.8,-273.2,31.8,26.9,0x00,0x00,972,SUCCESS 48,2023-01-23 14:04:38,192.021,0x0701,20,10,0x6001,0,65535,65535,1,31.8,27422,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3367,3434,3431,3451,3453,3388,3460,3436,0,0,0,0,0,0,0,3427,26.9,31.8,-273.2,31.8,26.9,0x00,0x00,970,SUCCESS 49,2023-01-23 14:04:42,196.021,0x0701,20,10,0x6001,0,65535,65535,1,31.8,27410,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3366,3432,3431,3448,3451,3387,3459,3435,0,0,0,0,0,0,0,3422,26.8,31.8,-273.2,31.8,26.8,0x00,0x00,972,SUCCESS 50,2023-01-23 14:04:46,200.022,0x0701,20,10,0x6001,0,65535,65535,1,31.8,27400,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3366,3431,3429,3446,3449,3386,3457,3433,0,0,0,0,0,0,0,3422,26.8,31.8,-273.2,31.8,26.8,0x00,0x00,973,SUCCESS 51,2023-01-23 14:04:50,204.023,0x0701,20,10,0x6001,0,65535,65535,1,31.8,27389,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3365,3429,3426,3446,3448,3385,3455,3431,0,0,0,0,0,0,0,3422,26.8,31.8,-273.2,31.8,26.8,0x00,0x00,969,SUCCESS 52,2023-01-23 14:04:54,208.023,0x0701,20,10,0x6001,0,65535,65535,1,31.8,27382,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3365,3427,3425,3446,3445,3385,3455,3431,0,0,0,0,0,0,0,3422,26.8,31.8,-273.2,31.8,26.8,0x00,0x00,970,SUCCESS 53,2023-01-23 14:04:58,212.024,0x0701,20,10,0x6001,0,65535,65535,1,31.8,27374,0,0,100,100,100,1050,1050,65535,65535,65535,44,29200,0x40E0,0,0,100,0x0107,0x8000,0x10,0xC4,0x4A,0x00B0,0x0000,0x0000,0x0008,0x0000,0x0000,0x0000,0x0000,3365,3426,3422,3446,3445,3384,3453,3430,0,0,0,0,0,0,0,3417,26.8,31.8,-273.2,31.8,26.8,0x00,0x00,971,SUCCESS
Mon Jan 23 14:30:17 CET 2023 Device Version Info = 1e9b_3_00 BQZ Device Name = bq78350R3 BQZ Firmware Version = V3_00_BLD31 Design Capacity = 1050 Design Voltage = 3200 Specification Info = 0x1031 Manufacturer Date = 2022-12-22 Serial Number = 0x0100 Manufacturer Name = ES024105-04 Device Name = 22110100 Device Chemistry = F174 Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,RunTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,PendingEdv,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFStatAB,CellVolt1,CellVolt2,CellVolt3,CellVolt4,CellVolt5,CellVolt6,CellVolt7,CellVolt8,CellVolt9,CellVolt10,CellVolt11,CellVolt12,CellVolt13,CellVolt14,CellVolt15,ExtAvgCellVolt,TS1 Temp,TS2 Temp,TS3 Temp,CellTemp,FetTemp,CB_REST_Enable,CB_REST_Enable,LogRowTime(ms),LogStatus 1,2023-01-23 14:30:21,4.002,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29108,19,15,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x9000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3373,3688,3736,3768,3756,3441,3688,3673,0,0,0,0,0,0,0,3637,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,966,SUCCESS 2,2023-01-23 14:30:25,8.002,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29134,20,16,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x9000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3373,3693,3740,3776,3760,3441,3693,3678,0,0,0,0,0,0,0,3642,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,966,SUCCESS 3,2023-01-23 14:30:29,12.003,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29179,19,17,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x9000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3376,3696,3746,3762,3782,3442,3697,3682,0,0,0,0,0,0,0,3647,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,966,SUCCESS 4,2023-01-23 14:30:33,16.003,0x0701,20,10,0x6001,0,65535,65535,1,31.3,29193,19,17,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x9000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3376,3701,3750,3766,3771,3444,3702,3686,0,0,0,0,0,0,0,3652,25.1,31.3,-273.2,31.3,25.1,0x00,0x00,965,SUCCESS 5,2023-01-23 14:30:37,20.003,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29221,20,18,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x8000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3377,3705,3755,3771,3776,3445,3706,3690,0,0,0,0,0,0,0,3652,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,980,SUCCESS 6,2023-01-23 14:30:41,24.004,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29251,18,18,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x9000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3378,3709,3760,3775,3794,3446,3710,3694,0,0,0,0,0,0,0,3657,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,967,SUCCESS 7,2023-01-23 14:30:45,28.004,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29272,17,18,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x9000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3378,3712,3763,3779,3787,3447,3714,3697,0,0,0,0,0,0,0,3660,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,965,SUCCESS 8,2023-01-23 14:30:49,32.004,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29287,14,17,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x8000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3377,3714,3765,3781,3786,3450,3716,3700,0,0,0,0,0,0,0,3661,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,964,SUCCESS 9,2023-01-23 14:30:53,36.005,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29300,13,16,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x8000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3378,3717,3767,3783,3789,3448,3718,3702,0,0,0,0,0,0,0,3661,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,962,SUCCESS 10,2023-01-23 14:30:57,40.006,0x0701,20,10,0x6001,0,65535,65535,1,31.2,29311,12,15,100,100,100,1050,1050,65535,65535,0,4000,29200,0x0080,0,0,100,0x0107,0x8000,0x10,0x08,0x10,0x00B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3378,3718,3769,3785,3791,3447,3720,3703,0,0,0,0,0,0,0,3666,25.1,31.2,-273.2,31.2,25.1,0x00,0x00,963,SUCCESS 11,2023-01-23 14:31:01,44.006,0x0701,20,10,0x6001,0,65535,65535,1,31.1,29325,11,15,100,100,100,1050,1050,65535,65535,0,4000,29200,0x4080,0,0,100,0x0107,0x9000,0x10,0x08,0x10,0x00B0,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3378,3720,3771,3787,3808,3449,3721,3705,0,0,0,0,0,0,0,3666,25.0,31.1,-273.2,31.1,25.0,0x00,0x00,961,SUCCESS 12,2023-01-23 14:31:05,48.006,0x0549,20,10,0x6001,0,65535,65535,1,31.1,29304,0,0,100,100,100,1050,1050,65535,65535,65535,0,0,0x00C0,0,0,100,0x4905,0x8000,0x10,0x08,0x40,0x00B0,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,3377,3717,3768,3784,3790,3447,3718,3702,0,0,0,0,0,0,0,3661,25.0,31.1,-273.2,31.1,25.0,0x00,0x00,976,SUCCESS 13,2023-01-23 14:31:09,52.007,0x0549,20,10,0x6001,0,65535,65535,1,31.1,29288,0,0,100,100,100,1050,1050,65535,65535,65535,0,0,0x00C0,0,0,100,0x4905,0x8000,0x10,0x08,0x40,0x00B0,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,3376,3714,3765,3782,3787,3446,3716,3699,0,0,0,0,0,0,0,3661,25.0,31.1,-273.2,31.1,25.0,0x00,0x00,978,SUCCESS