Other Parts Discussed in Thread: TPS65982, , TPS65987
I have a USB 2.0 device connected to the mux on the TPS65982-EVM through the header pins and have been unsuccessful getting the USB 2.0 bus to enumerate. I have been trying to configure the TPS65982 with the TI TPS6598X Application Customization tool over i2C as a source and UFP (this will be the only configuration used). The error message I see is:
[23944.521109] usb 1-1: new low-speed USB device number 120 using xhci_hcd
[23944.653304] usb 1-1: device descriptor read/64, error -71
[23944.893202] usb 1-1: device descriptor read/64, error -71
[23945.129245] usb 1-1: new low-speed USB device number 121 using xhci_hcd
[23945.257233] usb 1-1: device descriptor read/64, error -71
[23945.497129] usb 1-1: device descriptor read/64, error -71
[23945.605456] usb usb1-port1: attempt power cycle
[23946.017136] usb 1-1: new low-speed USB device number 122 using xhci_hcd
[23946.017785] usb 1-1: Device not responding to setup address.
[23946.225741] usb 1-1: Device not responding to setup address.
[23946.433127] usb 1-1: device not accepting address 122, error -71
[23946.569230] usb 1-1: new low-speed USB device number 123 using xhci_hcd
[23946.569876] usb 1-1: Device not responding to setup address.
[23946.777523] usb 1-1: Device not responding to setup address.
[23946.985190] usb 1-1: device not accepting address 123, error -71
[23946.985442] usb usb1-port1: unable to enumerate USB device
Please provide a configuration or some advice on what I should try next. Thanks as always!!