Hi,
I am looking to potentially use the TPS4811-Q1 for a high side driver however one of the requirements is to have firmware adjustable current limit for each channel
Initially looking at this part I was hoping to use the built in functionality without using external current sense and parts. I attempted to do this by replacing RIWRN with a voltage controlled resistor however I need more information on the current sensing and over-current protection circuit.
What is the Vref that IWRN pin voltage gets compared to? and What is the maximum and minimum current output on IWRN and IMON?
Secondly do you have another suggestion how to make this over current protection level adjustable? Without the need for a complete external circuit.