Other Parts Discussed in Thread: BQ24004
Hi team,
In the datasheet table 7-2, it is said that 11k ohm resistor is used to set 7.00V for 2 cell LiFePO4.
Can my customer use 11k ohm to set 7.00V for 2 cells Li-ion battery?

Regards,
Ohashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
In the datasheet table 7-2, it is said that 11k ohm resistor is used to set 7.00V for 2 cell LiFePO4.
Can my customer use 11k ohm to set 7.00V for 2 cells Li-ion battery?

Regards,
Ohashi
Hi John
Belows are the customer's use case.
[Use case]
・Configuration: 2 series lithium-ion battery for backup power supply
・Vin: 8V(7.79~8.53V)
・charging voltage: 7V
・charging current: 800mA
・discharging current: max650mA
・discharging time: 40sec
・battery capacity: 7.22mAh
They would like to set the charging voltage to 7V with 2 series Li-ion battery configuration. So, they thought that they should place 11k ohm resistor to VSET.
Regards,
Ohashi
Hi Ohashi
We think it will work form the BQ25171 standpoint:
The batteries will charge to 7V and current will decrease to termination value and unit will enter charge complete --- 171 will see what it expects from a LiFePO4 for charge cycle.
V-BAT_LOWV 2.0V vs 2.8V.
V-BAT_SHORT 1.2V vs 2.2V.
V-OUT_OVP 104% of VSET – when the battery is inserted it could indicate a fault (4.2V vs 3.0V).
BUT not sure how the battery will preform only charged to 3.5V per cell -- need to evaluate this.
Is battery capacity 7.22mAh or 7.22Ah?
Hi Johns
Thanks for the comments.
"V-BAT_LOWV 2.0V vs 2.8V."
Does this vs mean: V-BAT_LOWV is 2.0V for LiFePO4 and 2.8V for Li-ion battery?
For your question, the battery capacity is 7.22mAh.
Regards,
Ohashi
Hi Ohashi
Yes -- "V-BAT_LOWV is 2.0V for LiFePO4 and 2.8V for Li-ion battery?"
Hi Bill,
Thanks for your reply.
BTW, what would be the other recommended battery charger when they fail to use BQ25171-Q1?
[Use case]
・Configuration: 2 series lithium-ion battery for backup power supply
・Vin: 8V(7.79~8.53V)
・charging voltage: 7V (< 7.365V = Vin_min:7.79V – VDD_typ:0.425V)
・charging current: 800mA
・discharging current: max650mA
・discharging time: 40sec
・battery capacity: 7.22mAh
Regards,
Ohashi
Hi Ohashi
Take a look at the BQ24004 / 005 / 006.
They are Dual Cell Linear chargers, highly integrated solutions. Drop out voltage is about 0.5V.