This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170EVM-BIDIR: LM5170-Q1- Boost Operation_Load

Part Number: LM5170EVM-BIDIR
Other Parts Discussed in Thread: LM5170

Hello

I am using LM5170EVM-BIDIR, My system is to provide 24 V at LV port and load of 10 ohm resistor at HV port. I am using resistor of 10 ohm instead of E-load. Do it will make any changes in the parameters. What paramerters do I need to keep in consideration. My output would be 6 A, 48 V. 

Thanks