This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5021: Skip cycle bypass

Part Number: LM5021


I want fixed frequency over the load variation from 0 to 1.5A (Bypass skip cycle) . So I added resistor from VCC pin to CS pin as per datasheet Figure 14 Typical Application Circuit  and equation (24), R22 resistor is 10Kohm and R21 is 620k (Also checked with 100ohm, 6.2Kohm combination). But still I am not getting fixed frequency refer attached waveform. CH1 gate waveform, CH2-CS pin, CH4-VCC. 

*FYI cap connected to CS pin is 150pF.

Can you please confirm the waveform attached is correct. Why I am not getting fixed offset voltage at CS pin even VCC is fixed ~8V. 

Vin: 88 to 280Vdc,

Vout: 13.5Vdc,

Load: 20W,

Fsw: 100KHz.