Hi, BQ24800 support team
As for the deglitch time of ACOK_DRV, The datasheet is mentioned that
–Rising deglitch time : 1st plug-in after POR is 150msec, but the subsequent plug-in is 150msec or 1.3sec, depending on REG0x37[12]
–Falling deglitch time : 3usec
The below is a figure created based on the description of deglitch time of ACOK_DRV. It is the situation at first plug-n.
1. Which of #1 or "2 is correct as BQ24800 design? Or, is both wrong?
And one more question
2. Is deglitch time reset whenever ACDET drops lower than VACOK_FALL?
Thanks
Tamio