Hello:
We have a 65W USB-C PD ACF with UCC28782ADRTWR ac-dc circuit finally fully operational up to 65W output.
Our intention is to productize it for USBC PD AND a versatile charger.
The base design with UCC28782 shows a WT6636F USB interface chip .
We face a issue and the board broke @ 265VAC by lowering the load gradually to 1.15A. The oscilloscope signals (Drain LS) and the thermal were normal at the time of the break, around 40°C for the hottest point. There was no false manipulation on our part, the test environment was stable and known.
Visual inspection of the board shows no obvious failure. And GaN looks intact.
Finally, it is found that the BSW pin of the IC UCC28782 is damaged, and it can work normally again after replacing a new IC UCC28782 .
Two things need your help,
1.Please help review the SCH
2.What are the possible reasons that can cause the IC UCC28782 BSW pin to damaged ?
(The attachments are circuit and design calculator and used components)

UCC28782 Excel Design Calculator RevC 的202316.xlsx