Part Number: BQ21040EVM-777
Other Parts Discussed in Thread: BQ21040
Hi team,
In the User's Guide p4, it is said "Install the jumper on JP3 (TS) adjust R7 until VTS (voltage between TPS and GND) is around 1.23 V. Charging should be suspended. Reduce voltage on TS pin by adjust R7 until charging resumes. Further reduce the voltage on TS until VTS is around 278 mV and charging should be suspended".
But when we checked TS pin, VTS is max 0.298V and min 0.18V even if we adjust R7.
Do you have any idea as to cause of upper phenomenon?
The test condition is below.
Vin:5V
J1 to J4:same user's Guide 4.2
J5: open
JP1:open
Jp2:connect CHG-OUT
JP3:connected
R2:Adjusted to be TP7-GND resistance is 4.5ohm(ISET 120mA)
Best regards,
teritama