Hi,
for one of my projects, I am using a Load switch for 3.3 after that LM3691 regulator to stepdown to 1.8V. due to more rise time, the complete 3.3V generates after 1.8 V at the output, as the enable is tied to Vin of regulator, once the load switch passes 1.8 and some mV, 1.8V generates and power on the respective blocks,
hence want to add a delay circuit at the enable pin of regulator,
can you please suggest any circuits, so i can add-in delay generating 1.8V, so load switch is ready with 3.3V fully functional.
some startup delay ideas
regards