Hi,
For initial testing, we plan to power up TPS50601A-SP with no load. Input voltage to the device will be 5 V. Just to confirm: the device can regulate down to zero load or is a minimum load required?
According to the datasheet, "The total operating current for the device is approximately 5 mA when not switching and under no load. When the device is disabled, the supply current is typically less than 2.5 mA." It seems like the device is able to regulate with no load? If so, I should be expecting the device to draw around 5 mA from the source under no load condition, is that correct?
Thank you,
Fernando