Other Parts Discussed in Thread: BQ25995
We are using this part on a portable medical device for power path management and charging a single cell Li Ion battery. The charger and primary power supply to the medical device is a 5V DC output wallmount adapter. The battery pack is internal to the device. The battery pack has a thermistor which communicates temperature information to the IC.
At a high temperature above 45C on the battery pack, the BQ25995 IC seems to be cutting off the battery from the system and we are seeing a black out when external power is removed.
When scope waveforms are examined, we believe that the BATFET is being turned off by the IC, thereby isolating the battery and preventing it from providing power to the system.
I am looking for some guidance to resolve this issue since I am unable to find any explanation or solution in the datasheet. Section 8.2.7.5 of Datasheet says charging would be suspended at the high temperature threshold, but does not say anything about BATFET cutting off. Thermistor temperature is well below the BHOT threshold where BATFET is supposed to cut off to protect the battery from discharging at high temperature.


Will get you a capture with same parameters at high temperature charge suspend threshold.
Same signal capture as above, except at high ambient temperature of 43C. It shows that the VSYS cuts off a few milliseconds after VBUS is removed.






,