Other Parts Discussed in Thread: BQ25890,
Hello TI,
What is the difference BQ25890 & BQ25895, which one is the recommended for new design.
Thanks,
Rahul.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rahul,
The two devices are very similar. The main difference is that the BQ25895 is designed for OTG output at PMID instead of VBUS. This can be useful for battery pack applications or similar systems. BQ25895 also has an OTG output current of 3.1A (the BQ25890 has 2.4A OTG output).
See the sections called "Typical Application" in both datasheets for a visual of the differences.
Also take a look at Selection of Single-Cell Buck Narrow VDC Switching Battery Chargers for more information on our catalog.
Regards,
James