Hello,
In reading through the feedback on the TPSM63606, it states you can connect to VOUT at the desired point of regulation. I was planning on routing the feedback resistors and cap near the device, but then was going to route a differential trace on VOUT/GND closer to the load. Do you see any concerns with this approach?
I will have some local caps to generate a small plane near the device but my main load is a couple of inches away and wanted to provide better regulation at this point. This part doesn't feature a true remote sense so I wanted to ask.