I want to simulate ripple caused by load fluctuation.
I want to do a simulation that changes the load like 5V/5A -> 5V/8A -> 5V/5A
(Image USB type c load)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is this in PSpice or in WeBench?
In PSpice, you will need to add a Current Source to the load, either a Piece Wise Linear current Source or a Pulse current Source.
Set the loading resistor for 1Ω (5A @ 5V) and the current source to create the 2A loading transient that you are looking for.
In WeBench, under Simulate, select the "Load Transient" option.