This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS652170: PMIC with battery management

Expert 3931 points
Part Number: TPS652170
Other Parts Discussed in Thread: TPS6521815, TPS65217

Can you please recommend a PMIC with battery management features similar to the EFP0104GM20-D for a coin cell 2032 battery? 

Thanks!

  • Hello, 

    It does not appear we have a PMIC that closely matches the EFP0104GM20-D. Can you please help to specify the key features or requirements you are looking for?

    The TPS65217 has a built in battery charger, while the TPS6521815 is designed to work with a 2032 coin cell battery as a backup input supply. 

    Regards,

    Garrett 

  • If using a discrete battery management IC, do you have any recommendations for powering EFR32 and EFM32 devices? 

    Thanks!

  • Hi JDJ, 

    We do not have any PMICs specifically designed to power the EFR32 or EFM32, nor do we have collateral to showcase any of our existing PMICs powering this family of devices. 

    If you could help to provide the power requirements for the EFR32 and EFM32 devices I can suggest which of our PMIC options is the best fit. 

    Best Regards,

    Garrett