Hello
I am using LM5170EVM-BIDIR as a BOOST, My system is to provide 24 V at LV port and load of 10 ohm resistor at HV port. I have few complications:
1. I need to measure the duty cycle value which I think in board there is no test point. What is the best way to get the duty cycle measurents?
2. I also need to measure the inductor currents, which I read in data sheet that IOUT1 and IOUT2 pins are the input currents monitor pins which is inductor currents in case of BOOST operation but that are filtered one in EVM board. What is the possible way to get the inductor currents?
Thanks