This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25505: Battery voltage with 1.5 to 2.7v rating

Genius 13739 points
Part Number: BQ25505
Other Parts Discussed in Thread: BQ25570,

Hi Experts,

We would like to ask if the BQ25505RGRT charger IC does support battery rated 1.5 to 2.7V.
Is it possible for this rechargeable rating?

Thank you.

Regards,
Archie A.

  • Hi Archie,

    BQ25505 cannot be set for constant voltage less than 2.1V, which is the undervoltage setting.  Some customers get around this by using BQ25570 and connecting the battery to the buck converter output.

    Regards,

    Jeff