Hi Team,
Please find the mentioned below query:
Hi Team,
We are trying to read the Current & Voltage through PMBus and mentioned below commands we are using for the Reading the Voltage & Current.
Regulator Design parameters, Vin=12V, Vout=0.8V Iout= less than5.5A
Observations:
Voltage Read Commands:
(8Bh) READ_VOUT---> 0C82H(value)
(20h) VOUT_MODE--->82H(value)
Current Read Commands:
(8Ch) READ_IOUT--->0C42H.
Query:
1. Can we have some formula to convert the reeded value of Voltage and Current? Can give some examples to convert the reeded value into voltage & Current format.
2. For Voltage check, what exponent value should be used for calculating voltage. even as per datasheet recommendation, exponent value need to write the getting the correct the voltage. but we are getting failure at the time of writing.
3.For Current check, how to calculate current. it contains both the exponent and the mantissa. please give some examples for conversion of reeded value.
Thanks & regards,
Prasad Tatar