I'm trying to run a learning cycle on my LP-502535-1S-3 3.7V 400mAh 1.48Wh battery.
I have obtained a ChemID based on sluuc94.pdf.
I'm following your slua093.pdf document for the learning cycle. Everything went ok until stage 3.2.5, discharging to empty.
But at stage 3.2.6, even though REST was achieved, VOK did not clear and the Update Status did not update from 0x05 to 0x06.
I'm discharging with a ~56ohm resistor, so my discharge current is in the range of -70mA when the battery is fully charged to ~-40mA when nearly empty, at 2.75V.
I have run a learning cycle on a very similar battery with the exact same charging and discharging conditions before and then everything went ok.
Why would the status not update to 0x06?
The register and data memory logs are attached in the RAR file.
Thanks,