Hi Expert,
My customer is using BQ25601D in their project. They are testing termination current and found the actual current is larger than the threshold. The details are shown below:
Temp | Pre-charge current | Termination-voltage | Charge current | Termination-current | Threshold |
5℃ | 55mA | 4.41V | 845mA | 152mA | 120mA |
15℃ | 53mA | 4.41V | 1840mA | 147mA | 120mA |
25℃ | 56mA | 4.41V | 1840mA | 135mA | 120mA |
I checked the DS of BQ25601D, the measured current accuracy is slightly lower than the spec. Is that normal? Or should we judge by the worst accuracy regardless of the charging current?
BR,
Jiaqi Wang