Hi,
I would like to have technical assistance for a design using that components TPS54821, we want confirmation that will be working properly as the simulation is telling on TI tool, we try to generate levels of tension that we are not used to using, so we want to get from 15v to 10.5v 0.8A, and from 15V to 8.2V to 0.6A, and from 12V to 6V 3.68A, do you maintain NDA with our company Globalfoundries ?
I can share with you our designs