Hi Teams.
Could you tell me the maximum voltage on the SS pin?
conditions
VIN=16V
VOUT=1.0V
If you need more information, please let me know.
I'll use the information for Css selection.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Teams.
Could you tell me the maximum voltage on the SS pin?
conditions
VIN=16V
VOUT=1.0V
If you need more information, please let me know.
I'll use the information for Css selection.
Hi, if you would choose Css for soft start time calculations, just follow formula 2 in page 11. The time used for internal Iss charge Css to Vref is soft start time.
Yuchang
Hi, thank you for your reply.
Does that mean the maximum voltage on the SS pin is 0.6 V?
Relates to rated voltage in Css selection.
Hi Tomohisa
You can see the 7.2 functional block, actually, there is a 5uA internal current source(Iss) to charge the external Css cap, soft start ends after charging to 0.6V. The 0.6V is the Vref voltage and the soft start end point, not the max ss voltage. The Css calculation is based on Iss and Tss and don't need SS voltage.
xueliang
Hi, thank you for your reply.
I need to know the maximum SS voltage for Css selection.
Because Css has rated voltage.
The rated voltage of Css must be greater than the maximum SS voltage.
Could you tell me the maximum SS voltage?
Tagami
Hi Tomohisa
The max SS voltage is ~5V and the ABS value is 6V. recommend that the selected voltage not exceed 6V.
xueliang
Hi, thank you for your reply.
I'll select a capacitor with a rated voltage of 6V or higher for Css.
Tagami